SRIO Driver for MPC8641d

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SRIO Driver for MPC8641d

1,424件の閲覧回数
shrikantkumar
Contributor I

I am trying to develop SRIO driver for MPC8641d.

Currently i am able to send and receive doorbell messages correctly

So it means there is no issue with the backplane connectivity

But sending & Receiving of Data is not working. What could be the possible reason for this?

タグ(1)
0 件の賞賛
返信
1 返信

1,297件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at attached files. This attachment contains SRIO for Linux BSP for the MPC8641:

https://www.nxp.com/webapp/Download?colCode=CWF-MPC8641&appType=license

 

See description in the .html file and driver codes.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信