Reliable JTAG system adapter for MPC8314

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reliable JTAG system adapter for MPC8314

2,722件の閲覧回数
okernytskyy
Contributor II

Can anybody suggest a reliable JTAG system adapter for MPC8314?

It will be good if it will fit Molex connector p/n 87831-1420 (CONN, HEADER, 14POS, 2MM, VERT).

Pins assignment is attached.

2 返答(返信)

2,538件の閲覧回数
okernytskyy
Contributor II

Pavel,

Thank you for your help and information. I contacted NXP over the phone, posted on company web-site, and suggested E-mail address: [email protected] with intention to buy appropriate debugging tools, but did not receive any response yet so far.

0 件の賞賛
返信

2,538件の閲覧回数
Pavel
NXP Employee
NXP Employee

We recommend using CodeWarrior 8.8 compiler and CodeWarrior TAP or USB TAP for the MPC8314.

See the following pages:

http://www.nxp.com/products/developer-resources/software-development-tools/codewarrior-development-t...

 

and

 

http://www.nxp.com/products/developer-resources/software-development-tools/codewarrior-development-t...

 

and

 

http://www.nxp.com/products/developer-resources/software-development-tools/codewarrior-development-t...

 

See the Chapter 9 about CodeWarrior TAP connector for the MPC8314.

http://www.nxp.com/docs/en/user-guide/CWTAPUG.pdf

 

See also schematic for probe Tips for Power Architecture® processor (COP) CodeWarrior TAP:

https://www.nxp.com/webapp/Download?colCode=CWH-CTP-COP-YE-SCH&appType=license&Parent_nodeId=1347552...

 

and

 

https://easyeda.com/levanninh0101/component/HDR2X8-NqGECmI3N


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------