Reading Chip output pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reading Chip output pins

1,198 Views
maheshsubramani
Contributor I

Hi,

We are using MPC5775K and did not wire the CLKOUT0 and CLKOUT1 output pins.

By coding , is it possible to map  those outputs to GPIO ? if so, how ?

THanks

0 Kudos
Reply
1 Reply

1,136 Views
Pavel
NXP Employee
NXP Employee

These signals cannot be assigned to different pins.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply