When looking at the P2020 QorIQ Integrated Processor Reference Manual (Rev. 2, 12/2012), I notice that when the local bus is in bypass mode, eLBC drives new address, data, and control signals effectively on falling edges of LCLK, but continues to sample synchronous read data on rising edges of LCLK to maximize the set-up margin for reads. However, the precise timing relationship between TA signal and read-write signal is not clearly stated. 
I need to do an accurate timing analysis, but I don't know the specific timing relationship between TA signal and read-write signal, and which rising edge of LCLK is the sampling point for reading data when TA signal is asserted. 
The register settings in my design are as follows:
BR:0xd0001001
OR:0xffff0ef5
Any help would be much appreciated.
Thanks.
已解决! 转到解答。
Please refer to the P2020 QorIQ Integrated Processor Hardware Specifications, 2.12.2.3 Local Bus AC Timing Specifications for PLL Bypass Mode:
https://www.nxp.com/webapp/Download?colCode=P2020EC&location=null
I have read the p2020ec, but I still haven't figured out the exact timing relationship between the sampling point of reading data and the reading signal. At the same time, the time when writing data becomes invalid is related to the accurate timing of writing signal.
Can you give me a further explanation on the attached figure?
Thank you.
P2020 QorIQ Integrated Processor Reference Manual, 12.4.1.7 PLL Bypass mode:
"In PLL bypass mode, eLBC drives new address, data, and control signals effectively on falling edges of LCLK, but continues to sample synchronous read data on rising edges of LCLK to maximize the set-up margin for reads."
In the P2020 QorIQ Integrated Processor Hardware Specifications, 2.12.2.3 Local Bus AC Timing Specifications for PLL Bypass Mode:
Thank you for your reply.
According to your description, the sampling point for reading data should be the rising edge of lclk before the LOE is invalid, and at the next falling edge of lclk, LOE becomes invalid. Is my description right?
In addition, how about write timing?
> Is my description right?
Yes.
> In addition, how about write timing?
Please refer to the Figure 40 in the P2020 QorIQ Integrated Processor Hardware Specifications, 2.12.2.3 Local Bus AC Timing Specifications for PLL Bypass Mode.
In my design, OR register is set as follows:
| AM(0~16) | 17~18) | BCTLD(19) | CSNT(20) | ACS(21~22) | XACS(23) | 
| 0x1fff8 | 00 | 0 | 1 | 11 | 0 | 
| SCY(24~27) | SETA(28) | TRLX(29) | EHTR(30) | EAD(31) | 
 | 
| 1111 | 0 | 1 | 1 | 0 | 
 | 
According to P2020RM (Rev. 2, 12/2012) Table 12-191. GPCM write control signal timing parameters as follows:
| TRLX | XACS | ACS | CSNT | tAWCS | tCSWP | tAWE | tWEN | tWC | 
| 1 | 0 | 11 | 1 | 1.5 | 1.25+2* SCY | 2 | 0 | 2.75+2* SCY | 
But because TRLX = 1, so LCSn and LWE signals are negated one cycle earlier during Writes. The parameters in the above table will change to the following:
| TRLX | XACS | ACS | CSNT | tAWCS | tCSWP | tAWE | tWEN | tWC | 
| 1 | 0 | 11 | 1 | 1.5 | 0.25+2* SCY | 2 | 1 | 2.75+2* SCY | 
According to the above description, I have drawn the following timing diagram:
Is my description and timing diagram right?
I will be looking forward to your reply.
According to your help and my understanding of the P2020RM, I think the reading and writing sequence is as follows:
PLL bypass read timing:
The sampling point for reading data should be the rising edge of lclk before the LOE/LCS is invalid. This time is determined by the parameter tCSRP.
PLL bypass write timing:
Write data is invalid at the end of the tWC. This time is determined by the parameter tWC.
Is my understanding right?
I have another question:
As described in P2020RM, LCSn (only if ACS is not equal to 00) and LWE signals are negated one cycle earlier during Writes when TRLX is 1.
The write sequence will change from Figure 1 to figure 2?
Figure 1
Figure 2
If I use timing data from the corresponding row of the "Table 12-191. GPCM write control signal timing" without any modification.
| TRLX | XACS | ACS | CSNT | tAWCS | tCSWP | tAWE | tWEN | tWC | 
| 1 | 0 | 11 | 1 | 1.5 | 1.25+2* SCY | 2 | 0 | 2.75++2* SCY | 
Write timing diagram as following:
If it is the above timing, write data and write signal are invalid at the same time. so the hold time of write data will be insufficient.
And according to your comment, I am confused about the following description in P2020RM:
TRLX is 1:
Relaxed timing on the following parameters:
• Adds an additional cycle between the address and control signals (only if ACS is not equal to
00).
• Doubles the number of wait states specified by SCY, providing up to 30 wait states.
• Works in conjunction with EHTR to extend hold time on read accesses.
• LCSn (only if ACS is not equal to 00) and LWE signals are negated one cycle earlier during
Writes