P1014: using D_INIT multiple time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1014: using D_INIT multiple time

1,196 Views
renaud
Contributor IV

Is it possible to use D_INIT multiple time to write different pattern to the DDR memory? Goal is to write different pattern and read/compare.

~What would be the correct sequence to stop the memory and re-use D_INIT?

Cheers,

Renaud

0 Kudos
Reply
1 Reply

1,153 Views
ufedor
NXP Employee
NXP Employee

You wrote:
> Is it possible to use D_INIT multiple time
This is not possible. The data initialization is performed only once as described in the DDR_DDR_SDRAM_CFG_2[D_INIT] description in the P1014 QorIQ Integrated Processor Reference Manual.

0 Kudos
Reply