Need support for MC68360AI25L programmer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need support for MC68360AI25L programmer

1,220 Views
subas_hegde
Contributor I

I have newly procured a PE Micro systems Multilink Universal FX along with PROG32Z flash programmer software since the website said it can program. When I connect with hardware, It is asking for program algorithm (.32p format), but I couldn’t find one for 68360 controller.

Please help to get program algorithm for this tool or any other way to flash program using Multilink Universal FX.

Need your support at the earliest.

0 Kudos
Reply
1 Reply

1,113 Views
LPP
NXP Employee
NXP Employee

This programmer is not a product of Freescale/NXP. You must contact to PE Micro for support

P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools...

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply