NAND boot without CPLD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NAND boot without CPLD

1,303 Views
Irfan3
Contributor III

Hi Team,

We are using T2080RDB board. As per the manual for NAND boot, the SW3[4] should be one for selecting NAND and SW3[4] should be zero for selecting NOR.

Based on the Documents this pin is BOOT_SEL pin wrt to FLASH_SRC register and controlled by CPLD.

We are planning to remove CPLD in our custom board, so can we boot from NAND without using CPLD and sw3[4] which is used for boot media selection either by Hardware or software.

Can you please provide us valuable inputs to this query.

Thanks for your support.

Regards,

Irfan

0 Kudos
Reply
0 Replies