MPC885vr133 linux BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC885vr133 linux BSP

1,147件の閲覧回数
vadrevujyothi
Contributor I

Hi,

           I am using MPC885VR133 development board for Linux development. I have downloaded Linux BSP MPC885ADS. As mentioned in documents i have loaded planetcore bootloader. But i am not able to boot kernel image. Can you tell me how to ecxecute kernel image from boot loader. When i am trying to boot kernel image again boot loader only executing.

0 件の賞賛
返信
1 返信

1,035件の閲覧回数
Pavel
NXP Employee
NXP Employee

There is Linux BSP for the MPC885ADS board:

https://www.nxp.com/webapp/Download?colCode=CWF_MPC885ADS&appType=license&location=null&Parent_nodeI...

 

This BSP recommends using u-boot as boot loader.

Do you use the same BSP on your board?

See attachment.

Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信