MPC885vr133 linux BSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC885vr133 linux BSP

1,138 Views
vadrevujyothi
Contributor I

Hi,

           I am using MPC885VR133 development board for Linux development. I have downloaded Linux BSP MPC885ADS. As mentioned in documents i have loaded planetcore bootloader. But i am not able to boot kernel image. Can you tell me how to ecxecute kernel image from boot loader. When i am trying to boot kernel image again boot loader only executing.

0 Kudos
Reply
1 Reply

1,026 Views
Pavel
NXP Employee
NXP Employee

There is Linux BSP for the MPC885ADS board:

https://www.nxp.com/webapp/Download?colCode=CWF_MPC885ADS&appType=license&location=null&Parent_nodeI...

 

This BSP recommends using u-boot as boot loader.

Do you use the same BSP on your board?

See attachment.

Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply