MPC8640 Probe

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC8640 Probe

2,929 次查看
arun2
Contributor II

Hi ,

Please help me is there any suitable option for CWH-UTP-PPCC-HE

Regards ,

Arun K Soman

PME

WT Microelectronics

标签 (1)
0 项奖励
回复
3 回复数

2,290 次查看
alexander_yakov
NXP Employee
NXP Employee

The probe CWH-UTP-PPCC-HE is not available for ordering, but if you have it - it will work with MPC8640

If you need to order a new probe for this device, please other CodeWarrior TAP - partnumbers CWH-CTP-BASE-HE and CWH-CTP-COP-YE (base and JTAG/COP probe tip).

Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,290 次查看
arun2
Contributor II

Sir ,

I have two queries ,

What will be the tools (Tap and Probe ) which support below parts .

1.     MC8640DTVJ1250HE

2.     MPC8540

Regards ,

Arun K soman

PME

WT Microelectronics Singapore Pte Ltd

0 项奖励
回复

2,290 次查看
sinanakman
Senior Contributor III

Hi Arun

Freescale has a replacement probe called CWTAP that

you should be able to use with MPC8640.

We are using a Abatron BDI3000 probes here.

Hope this helps

Regards

Sinan Akman

0 项奖励
回复