MPC8548E PCIX, PCIe and sRIO

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC8548E PCIX, PCIe and sRIO

1,603 次查看
Des
Contributor I

Hi

Currently we use the MPC8548E and in our current design we use the PCI-X bus and sRIO (supporting 1.25, 2.5 and 3.125 Gbps).  Due to obselecense we are looking at changing one of the PCI-X bus devices with a PCIe device.  We would therefore be using the PCI-X bus, PCIe bus and sRIO. 

Looking at the documentation, this is possible by restricting both the sRIO and PCIe to x4 at a rate of 2.5Gbps.  Is this correct?  Are there any other issues I should be aware of when running PCI-X, PCIe and sRIO together. I just wanted to double check this before we respin the board.

0 项奖励
回复
1 回复

1,177 次查看
ufedor
NXP Employee
NXP Employee

Your understanding is correct.

There are no other issues.

0 项奖励
回复