MPC8548E Memory Map CCSR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC8548E Memory Map CCSR

2,577 次查看
axlmr
Contributor I

I have a question about the  CCSR Register

In the documentations says

“All of the memory mapped configuration, control, and status registers in the MPC8548E are contained

within a 1-Mbyte address region. To allow for flexibility, the configuration, control, and status block is

relocatable in the local address space.” ‘Section 2.3 Reference Manual.

What is the process to relocate this register? When and How it is done?

1 回复

2,102 次查看
scottwood
NXP Employee
NXP Employee

The process is documented in the "Updating CCSRBAR" section of the manual (4.3.1.1.1).  It is typically done during early boot if the default address isn't desired (e.g. if you want to use 4GiB or more of RAM, you'll want to move CCSR out of the way).  U-Boot has code to relocate CCSRBAR in arch/powerpc/cpu/mpc85xx/start.S.