MPC837x PCIe sample embedded driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC837x PCIe sample embedded driver

1,290件の閲覧回数
tuyen_nguyen
Contributor I

I start writing PCI Express driver code for the embedded system in which master embedded board is using MPC837x to communicate with other devices using PCIe . I have no experience in such driver and do not know where to start. Anyone can provide or point me to where I can find the basic PCIe driver of this processor MPC837x or similar one? Thanks

0 件の賞賛
返信
1 返信

1,229件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the U-Boot PCI driver source code and PCIe patches provided in the MPC837x MDS LTIB BSP:

LTIB BSP for MPC837x MDS 

0 件の賞賛
返信