MPC8323 rdb Jffs2 file system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8323 rdb Jffs2 file system

3,058件の閲覧回数
gangadharrao
Contributor II

I am unable to load JFFS2 file system into MPC8323 RBD board .Can anyone share inform how to use JFFS2 file system instead of RAMDISK which I am using now.

Using LTIB for JFFS2 file generation.

0 件の賞賛
返信
1 返信

2,900件の閲覧回数
Pavel
NXP Employee
NXP Employee

See attached file. Find deployment the jffs in this file.

See also attached screenshot for jffs2 setting in the ltib.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信