MPC8313RDB Boot Sequencer Tool ( i2c_bootseq_generator.c)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8313RDB Boot Sequencer Tool ( i2c_bootseq_generator.c)

1,760件の閲覧回数
malikali
Contributor I

Dear Experts,

I'm trying to generate the EEPROM content for the Boot Sequencer on MPC8313RDB and need access to the i2c_bootseq_generator.c source file as referenced in PowerQUICC III Bring-Up Guideline and MPC8568E Design Checklist to create a Boot Sequencer Tool to generate raw data format file that can be used to program the I2C EEPROM. I will really appreciate if anyone able to advise where I might be able to locate the boot sequencer tool source please?

If there is any other tool available to generate the I2C EEPROM content for MPC8313RDB Boot Sequencer then it would also help.

Best regards,

-Malik

0 件の賞賛
返信
1 返信

1,703件の閲覧回数
malikali
Contributor I

I would like to thank NXP Technical Support for a quick response to resolve the matter and emailing the BootSequenceTool.zip package.

I consider this issue resolved.

0 件の賞賛
返信