MPC8313ERDB ETSEC1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8313ERDB ETSEC1

3,103 Views
jamakh
Contributor I

HI,

I want to use ETSEC1 with Marvell PHY  instead of L2 switch.I have seen in user guide that some resistors need to be moved to some other location as shown in the attached document.I have done this. when  I connect  to G0  connector then Leds Rx,Dup light up but connector does not blink.Also for other connectors G1-G4  even no Led light up..If I use G0 and reads the PHY-ID register then I read zero..So any one can help? ETSEC2is working fine with me..

Thanks

Jam

Labels (2)
Tags (3)
0 Kudos
Reply
1 Reply

2,709 Views
lunminliang
NXP Employee
NXP Employee

See below technical support comment:

1) Which exactly RDB revision i in question? - What are all on-board inscriptions and markings?

2) Which exactly rework operations were performed?

Refer to the attached PowerQUICC™ MPC8313E Reference Design Board (RDB), Rev. 5.


0 Kudos
Reply