MPC8308NSG Routing table Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8308NSG Routing table Configuration

24,139件の閲覧回数
ziedjelassi
Contributor II

Hi,

I'm using ISP router modem to have an internet access. So it manages the 192.168.1.0/24 sub-network and provide internet access. I have linked the MPC8308NSG WAN interface to this router. As network.png figure shows; I have accorded to it the 192.168.1.96 address. And it will manages the 192.168.2.0/24 sub-network. Other linked figures show its firewall and routing table configurations.

I have linked a PC to MPC8308NSG LAN and I have tested internet access. the result is negative; any device in MPC8308NSG LAN cannot have see any address not in 192.168.2.0/24 sub-network.

Please help.

Best regards,

Zied.

26 返答(返信)

19,279件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Your "ISP router modem" should be also properly configured to be aware, where to route packets for network 192.168.2.0/24

Please configure modem router table to route network 192.168.2.0/24 to gateway 192.168.1.96


Also, your modem (I  guess) performs NAT (network address translation) for network 192.168.1.0/24 and I'm not sure if it is really possible to instruct this device to also perform this translation for network 192.168.2.0/24


Note, address 192.168.1.96 is dynamically allocated by your modem' DHCP service and may be changed.

Please look DHCP settings and configure permanent allocation.


With net.ipv4.ip_forward=1 in sysctl.conf this should solve the problem.

0 件の賞賛
返信

19,279件の閲覧回数
ziedjelassi
Contributor II

Hi,

the figures below describe the MPC8308NSG (called NSG-EBSYS) traceroute result and the host addressed 192.168.2.147 one.

terminal1.pngterminal2.png

Best regards,

Zied

0 件の賞賛
返信

19,279件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Please show kernel routing table in NSG

0 件の賞賛
返信

19,279件の閲覧回数
ziedjelassi
Contributor II

kernel routing table.png

0 件の賞賛
返信

19,279件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Routing table shows two networks 192.168.1.0 and 192.168.2.0 directly connected, network 192.168.2.0 listed two times with interfaces br-lan and ra00_0

So, as I can guess, you have configured IP addresses from the same network 192.168.2.0/24 on two different interfaces.

Please determine which one is correct, remove incorrect interface (or assign IP-address from another network).

Check the result by ping 192.168.2.147

Also, there are two "default" entries. This entry means where to send packets for all other networks, not listed explicitly in routing table.

In your case first entry is correct, NSG should send all other packets to 192.168.1.1 (your ISP router modem). Second entry should be removed.

Check the result by traceroute to any external internet address.

0 件の賞賛
返信

19,279件の閲覧回数
ziedjelassi
Contributor II

Hi Alexander,

the linked figure shows the MPC8308NSG ifconfig result:

132.png

the routing table presented below is the auto generated one.

Best regards,

Zied.

0 件の賞賛
返信

19,278件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

the routing table presented below is the auto generated one.

If this case please show source file from which this routing table was auto generated.

It can not be auto generated from ifconfig output.

0 件の賞賛
返信

19,278件の閲覧回数
ziedjelassi
Contributor II

Hi Alexander,

please can I know you routing table suggestion to be forced!

Best Regards,

Zied.

0 件の賞賛
返信

19,278件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

My suggestion to your routing table is above.

Here is a copy:

Routing table shows two networks 192.168.1.0 and 192.168.2.0 directly connected, network 192.168.2.0 listed two times with interfaces br-lan and ra00_0

So, as I can guess, you have configured IP addresses from the same network 192.168.2.0/24 on two different interfaces.

Please determine which one is correct, remove incorrect interface (or assign IP-address from another network).

Check the result by ping 192.168.2.147

Also, there are two "default" entries. This entry means where to send packets for all other networks, not listed explicitly in routing table.

In your case first entry is correct, NSG should send all other packets to 192.168.1.1 (your ISP router modem). Second entry should be removed.

Check the result by traceroute to any external internet address.

The fact that the table is auto generated does not mean this table is correct and does not mean it can not be changed.

The ifconfig output can not be used to generate routing table, the table is generated from other source which is obviously incorrect.

0 件の賞賛
返信

19,278件の閲覧回数
ziedjelassi
Contributor II

Hi Alexander,

Following your recommendations, I have act on my NSG routing table to be as shown in the attached figure

Sans titre.png

But, there is no changes.

Best regards,

Zied.

0 件の賞賛
返信

19,278件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

I still see two "default" entries in your table.

0 件の賞賛
返信

19,278件の閲覧回数
ziedjelassi
Contributor II

Hi Alexander,

I have checked these routing table configurations:

Destination     Gateway         Genmask         Flags Metric Ref    Use Iface

192.168.2.0     *               255.255.255.0   U     0      0        0 br-lan

192.168.1.0     *               255.255.255.0   U     0      0        0 eth1

default         192.168.1.1     0.0.0.0         UG    0      0        0 eth1

Destination     Gateway         Genmask         Flags Metric Ref    Use Iface

192.168.1.0     *               255.255.255.0   U     0      0        0 eth1

192.168.0.0     *               255.255.0.0     U     0      0        0 br-lan

default         192.168.1.1     0.0.0.0         UG    0      0        0 eth1

Destination     Gateway         Genmask         Flags Metric Ref    Use Iface

192.168.1.0     *               255.255.255.0   U     0      0        0 eth1

192.168.0.0     *               255.255.0.0     U     0      0        0 br-lan

default         192.168.2.1     0.0.0.0         UG    0      0        0 br-lan

Destination     Gateway         Genmask         Flags Metric Ref    Use Iface

192.168.2.0     *               255.255.255.0   U     0      0        0 br-lan

192.168.1.0     *               255.255.255.0   U     0      0        0 eth1

default         192.168.2.1     0.0.0.0         UG    0      0        0 br-lan

Destination     Gateway         Genmask         Flags Metric Ref    Use Iface

192.168.2.0     *               255.255.255.0   U     0      0        0 br-lan

192.168.1.0     *               255.255.255.0   U     0      0        0 eth1

default         192.168.1.1     0.0.0.0         UG    0      0        0 eth1

Sans titre.png

Sans titre1.png

But, Tell now, I haven't seen any changes.

Best regards,

Zied.

0 件の賞賛
返信

19,278件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

For 1 - please check the result by ping 192.168.2.147, please show the result.


For 2 - please check the result by traceroute to any external internet address, and show the result.

0 件の賞賛
返信

19,279件の閲覧回数
albertovargas
NXP Employee
NXP Employee

Hi zied

First of all, Have you set the default gateway to be 192.168.2.1 for computer 3?. I'm not familiar with MPC8308NSG, but, if you can, try pinging from 192.168.2.1 to 192.168.2.3 and from 192.168.2.3 to 192.168.2.1.

In the first case, if it's succesful, the problem could be the MPC8308NSG firewall rules. If it's not, disable any firewall in computer 3 and try again, especially if you're using Windows.

In the second case, the trouble could be in MPC8308NSG firewall configuration and again, try disabling any firewall in computer 3.

The last thing you can check is if you're using the correct cable, straight or crossover..

I hope this helps.

0 件の賞賛
返信

19,279件の閲覧回数
ziedjelassi
Contributor II

Hi Alberto,

computer 3 has as gateway address 192.168.2.1 and the ping service is ensured in both side as shown in my comment (ziedjelassi 17 sept. 2013 07:39 (en réponse à Sinan Akman)). All firewall are disabled. And my cables are checked.

networking service is restarted but tell now there is no changes.

Best regards,

Zied.

0 件の賞賛
返信

19,279件の閲覧回数
albertovargas
NXP Employee
NXP Employee

I think what may be happening, your computers in the 192.168.1.0 network side have their default gateway set to 192.168.1.1. When a packet addressed to 192.168.2.0 network arrives, 192.168.1.1 (ISP ROUTER) doesn't know what to do with it, because it doesn't know the 192.168.2.0 network. Try using a traceroute from both sides to see if that is what is going on.

0 件の賞賛
返信

19,279件の閲覧回数
ziedjelassi
Contributor II

Hi Alberto,

Thx for your answer.

I have disable computer 3 firewall but there is no changes.

Best regards,

Zied.

0 件の賞賛
返信

19,279件の閲覧回数
sinanakman
Senior Contributor III

Hi Zied, I am not familiar particularly with MPC8308NSG, but in general, first start testing from inside MPC8308NSG. Login to that device and ping a public address. If this works, then ping the address of MPC8308NSG (192.168.2.1 ??) from your PC. If that works as well then there is mainly two possibilities : either MPC8308NSG does not forward the ping or perhaps the ISP provided router is filtering the ping reply on the way back. So please test the ping separately e.g. : PC->MPC8308NSG, MPC8308NSG-> ISP router, PC->ISP Router, MPC8308NSG->Internet and finally PC->Internet. Hope this helps.

Sinan Akman

0 件の賞賛
返信

19,279件の閲覧回数
ziedjelassi
Contributor II

Hi Sinan,

Thx for your answer.

Drawing1.png

the linked figure shows our network.

the next table resumes the ping results.

--------------------------------------------------------------------------------------------------------------------------

Ping                        from                          To                               Status

--------------------------------------------------------------------------------------------------------------------------

                    192.168.2.3                    192.168.2.1                  ok

                    192.168.2.3                    192.168.1.96                ok

                    192.168.2.1                    192.168.2.3                  ok

                    192.168.1.96                  192.168.1.1                  ok

                    192.168.1.96                  192.168.1.3                  ok

                    192.168.1.96                   www.freescale.com      ok

                    192.168.2.3                    192.168.1.1                  NOK

                    192.168.2.3                    192.168.1.3                  NOK

                    192.168.2.3                    www.freescale.com       NOK

Best regards,

Zied.

0 件の賞賛
返信

19,279件の閲覧回数
sinanakman
Senior Contributor III

Hi Zied, it seems like your 8308 is not doing the forward. If you are running Linux on that box, you might try something like :

echo 1 > /proc/sys/net/ipv4/ip_forward


To enable ip forwarding. Check its value beforehand if it was disabled.    

Hope this helps.