MPC 8260 FEC Full Duplex Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC 8260 FEC Full Duplex Mode

2,462件の閲覧回数
cfernand
Contributor I

I am using the Fast Ethernet Controller (FEC) on the 8260.

The FEC FPSMR[FDE] bit controls full duplex mode.

The management lines (MDC and MDIO) to the phy are not connected.

Question is can  FDE be enabled for phy connections that are half duplex ?

I would like to enable FDE (Full Duplex) and be certain that this will work for both duplex connections.

 

-Carlos

0 件の賞賛
返信
4 返答(返信)

2,452件の閲覧回数
Pavel
NXP Employee
NXP Employee

 

Your PHY will generate collision if the MPC8260 FCC is configured in full-duplex.

0 件の賞賛
返信

2,444件の閲覧回数
cfernand
Contributor I

And because the FCC will ignore collisions in full duplex mode, no retries will occur.

Thank you.

 

0 件の賞賛
返信

2,436件の閲覧回数
Pavel
NXP Employee
NXP Employee

Check collision and carrier sense events in your PHY datasheet.

0 件の賞賛
返信

2,433件の閲覧回数
cfernand
Contributor I

The question is more about what the FCC/CPM does with collisions in full duplex mode.

I believe I found the answer in the user manual where it states that collisions are ignored in full duplex mode. It seems that to work properly, the FCC duplex mode must be set according to the established link mode.

0 件の賞賛
返信