MPC 8250 SCC, Transparent Synchronous Operation?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC 8250 SCC, Transparent Synchronous Operation?

1,373件の閲覧回数
caryo_brien
Contributor III

We have a low-speed wan bridging requirement that needs the scc on a mpc8250 to run in transparent synchronous mode. Ideally we would be able to use a Linux driver for this.  There are drivers for hdlc mode, but not for unframed/transparent mode.  Any idea where I could find such a thing?  Or what I should use for a starting point?

0 件の賞賛
返信
1 返信

1,278件の閲覧回数
Pavel
NXP Employee
NXP Employee

The MPC8250 SCC in transparent mode provides data transfers. Each clock can be supplied from the internal baud rate generator bank, DPLL output, or external pins. The SCC transparent data transfers is synchronous data transfers.

What Synchronous Operations are needed for your task?

Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信