MLC NAND Support for P1021 with SDK1.7 release

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MLC NAND Support for P1021 with SDK1.7 release

Jump to solution
1,486 Views
shubhasingh
Contributor I

Hi,

Can anyone clarify me regarding the MLC nand driver support with the kernel 3.12 for P1021 released with SDK 1.7 QorIQ.

Thanks,

Shubha

Tags (1)
0 Kudos
Reply
1 Solution
1,352 Views
lunminliang
NXP Employee
NXP Employee

Hello shubha singh,

For P1021, FCM does not support MLC NAND as its ECC requirement, it works if software ECC used.

And as I remember Freescale SDK does not include software BCH ECC, I'll confirm further if this is the case for 1.7.


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,353 Views
lunminliang
NXP Employee
NXP Employee

Hello shubha singh,

For P1021, FCM does not support MLC NAND as its ECC requirement, it works if software ECC used.

And as I remember Freescale SDK does not include software BCH ECC, I'll confirm further if this is the case for 1.7.


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,352 Views
shubhasingh
Contributor I

Thanks, lunminliang

I am planning to add the BCH ECC support for 4 bit ECC, could you please provide me some information on this.

Regards,

Shubha

0 Kudos
Reply