LS1028A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1028A

2,809 Views
mkraj
Contributor III

Dear NXP Team

1. We have developed a custom board based on LS1028A and want to use tamper input  feature of it

2. How TA_TMP_DETECT_B and TA_BB_TMP_DETECT_B are used by the LS1028A internally. These things are not mentioned in the user manual

3. We are driving these pins externally. Is there any literature to implement these tamper applications on LS1028A.

4. We are also planning to use MCU MK81FN256VLL15 for tamper application. How these are different from MK24FN1M0VLQ12. Is it ok to use MK24FN1M0VLQ12.

Thank you,

With Regards

Krishnam Raju M

2 Replies

2,790 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello @mkraj 

Hope this email finds you well,

This post is to inform you that in order to provide the requested information, please create a new ticket using the technical support web located in the following link:
https://support.nxp.com/s/

Also, kindly let us know on the new ticket your active NDA number or file.

Have a great day.
Best Regards,
Hector Villarruel

0 Kudos
Reply

2,780 Views
mkraj
Contributor III

Dear Hector Villarruel

Thank you.

With Regards