JTAG programming for MPC8358E

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JTAG programming for MPC8358E

2,138件の閲覧回数
danilicstibor
Contributor I

I am very confused about the programmers compatible with MPC8358E.

The site gives link to programmers (for ex: pemicro cyclone) that do not support this processor based on the details on the

webpages and datasheets.

This is serious misinforming.

Please help me, which one i should choose? I need for production enviroment.

I have an older Codewarrior USB TAP but that is broken, and it was barely used, so i would not buy again ever.

Even the current USB TAP does not list this device as compatible.

Something like the Cyclone would be great, but it looks like it's not compatible with MPC8358E.

I will program thru jtag some flashes connected to this processor, of course, not the processor itself.

Please help.

Thanks.

3 返答(返信)

1,940件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Old "USB TAP" is no longer available for ordering, please use "CodeWarrior TAP" (previously known as "Ethernet Tap").

CodeWarrior TAP|NXP 

Please do not forget to order JTAG/COP probe tip for this TAP.

Power Architecture processor for CodeWarrior|NXP 

Sorry, we do not offer a solution for factory production programming, we offer only CodeWarrior (for development)

0 件の賞賛
返信

1,940件の閲覧回数
sinanakman
Senior Contributor III

Hi Danilics

We use here BDI3000 from Abatron. The product is EOL'ed but it seems

there is still some available in stock. The manual lists 8358 as one of the

supported cpu types.

Hope this helps.

Sinan Akman

1,940件の閲覧回数
danilicstibor
Contributor I

Sorry, i just verified again and CW TAP looks like it is compatible.

What software is compatible and which is needed to run?

PEmicro confirmed that none of their devices supports MPC8358E.

Is there any other alternative for production?

Not for development.

Thanks!

0 件の賞賛
返信