Heat Spreader Implementation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Heat Spreader Implementation

2,870 Views
matthewware
Contributor I

The Datasheet for MPC8640D says that "In any implementation of a heat sink solution, the force on the die should not exceed to pounds force".

1. If say an additional 10% of force, or a total of 11lbs force, would the die be at a high risk of damage?

2. Is that limit a constant clamping force, or a one lime installation force limit?

3. What would the main failure mode be if excessive force was applied? (fail at High current, immediate failure, failure at temperature. etc.)

Thanks!

0 Kudos
Reply
2 Replies

2,773 Views
alexander_yakov
NXP Employee
NXP Employee

MPC8640D package has exposed silicon die (lidless). The main threats are cracking of the die because of package bending or non-parallel alignment of heat sink.

Under no circumstances shall the total load exceed 80 N. Maximum short-term dynamic tensile force should not exceed 15 N (1.5 Kg equivalent). Maximum short-term dynamic compressive force shall not exceed 70 N (7.1 Kg equivalent).
Long-term static tensile forces are not allowed. Maximum long-term static compressive force on the package shall not exceed 45 N.

Reference document:
http://cache.nxp.com/files/32bit/doc/app_note/AN4871.pdf

Note. Aplication note allows more force to be applied for this package. We provide conservative requirments in datasheet.


-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,368 Views
DanielDuJijun
Contributor III

Dear NXP Support Team.

Please help to share the download link for the following application note.

we cannot download AN4871 from the following link.

http://cache.nxp.com/files/32bit/doc/app_note/AN4871.pdf

0 Kudos
Reply