GPIO latch in T1022

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO latch in T1022

Jump to solution
1,266 Views
hemwant
Contributor IV

I am having a T1022 processor based board, one of the gpio signal GPIO3_31 is by default configured as output , i wanted it to be configured as GPIO3_31 as input. I have made the changes via GPIO direction register. But on giving reset to processor the pin again gets configured as output. Is there some way i can latch the value of the respective pin or modify the default configuration of the pin so that after reboot/reset of the same , the port pin configuration remains same as done at time of reboot/reset.

0 Kudos
Reply
1 Solution
1,242 Views
Bulat
NXP Employee
NXP Employee

As I wrote, all GPIO pins are configured as inputs at reset. This is a hardware feature and can not be changed. You can re-configure direction of GPIO pins in the boot code if you need.

Regards,

Bulat

 

View solution in original post

0 Kudos
Reply
3 Replies
1,260 Views
Bulat
NXP Employee
NXP Employee

All GPIO direction registers of the T1022 are set to 0x0 at reset (default value), so all GPIO ports are set as inputs. If you see that GPIO3_31 is set as an output, it was configured somewhere in boot code or PBL.

Regards,

Bulat

 

0 Kudos
Reply
1,251 Views
hemwant
Contributor IV

@Bulatyes the GPIO3_31 is configured as input by default when processor is given reset. I want it to be in output mode when it gets reset from linux. Is there some way to do that, so that i can retain the state of GPIO3_31 after reset?

0 Kudos
Reply
1,243 Views
Bulat
NXP Employee
NXP Employee

As I wrote, all GPIO pins are configured as inputs at reset. This is a hardware feature and can not be changed. You can re-configure direction of GPIO pins in the boot code if you need.

Regards,

Bulat

 

0 Kudos
Reply