Flash the code into external memory IDE CODE_WARRIOR v8.8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash the code into external memory IDE CODE_WARRIOR v8.8

1,436件の閲覧回数
maheshwarreddy
Contributor I

we are using processor MPC860 . we want to flash code into the external  memory NOR FLASH through USB TAP but the manufacturer parts are not available in the code warrior ide available   devices are absolute . so we went for new device but the device is not available for this how to flash the code into external memory.

Type of memory is NOR FLASH (1Megabits * 16).  

0 件の賞賛
返信
1 返信

1,374件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

For the documentation on how to add your own flash please look the following path:

[your CodeWarrior installation folder] \PowerPC_EABI_Tools\FlashProgrammer\Documentation\

0 件の賞賛
返信