Debugging DMA corruption - MPC8555 - Trace Buffers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugging DMA corruption - MPC8555 - Trace Buffers

2,289 Views
dijo
Contributor III

Hi Pavel,

we were able to locate the document and see the trace buffer  in action.

We were unable to find the right settings to trace a write over PCI/and through the Core to a DDR location (0x0eb00000) .

We tried using the following settings -

pastedImage_2.png

Do you see something which we overlooked, or did wrong?

Thanks in advance.

0 Kudos
Reply
2 Replies

2,052 Views
LPP
NXP Employee
NXP Employee

It's good but i suggest to set "trace only in TRACE event" flag.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,052 Views
dijo
Contributor III

Thanks again, Pavel!

Yes it works!

Would be great if you could tell how it works.What the "TRACE" implies?

0 Kudos
Reply