DRIVERS AND JTAG FOR MPC866

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DRIVERS AND JTAG FOR MPC866

2,602 Views
skchethan123
Contributor I

I am using MPC866 in which I have to work with SPI, UART and parallel bus. So can i know that where i can find the drivers for those peripherals. And i want to know which all the supported JTAG for MPC866 

Labels (3)
0 Kudos
Reply
3 Replies

2,447 Views
Pavel
NXP Employee
NXP Employee

See simple program examples in the attached file.

If there is a problem for .zip or 7z file loading, create please technical case:

https://community.nxp.com/thread/381898


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,447 Views
Pavel
NXP Employee
NXP Employee

See simple program examples in the attached file.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,447 Views
skchethan123
Contributor I

sorry Mr. Pavel I did not any attachments.

0 Kudos
Reply