Compatible JTAG probe for MPC885

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compatible JTAG probe for MPC885

ソリューションへジャンプ
3,195件の閲覧回数
visakhanc
Contributor III

Hi all,

     I have a project based on MPC885c PowerQUICK processor. What is the supported Codewarrior TAP and Probe part number for this processor? I have the base unit CWH-CTP-BASE-HE and probe tip: CWH-CTP-COP-YE. Are these compatible with MPC885 ?

Regards

Visakhan

0 件の賞賛
返信
1 解決策
3,002件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

MPC8xx (PowerQuicc 1) devices have another type debug interface - BDM

For these device please order the following debug probe:

USB TAP for DPI Power Architecture|Freescale

CodeWarrior TAP with COP-type probe tip CWH-CTP-COP-YE - will not work. BDM-type probe tip for CodeWarrior TAP - not available for ordering anymore.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,003件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

MPC8xx (PowerQuicc 1) devices have another type debug interface - BDM

For these device please order the following debug probe:

USB TAP for DPI Power Architecture|Freescale

CodeWarrior TAP with COP-type probe tip CWH-CTP-COP-YE - will not work. BDM-type probe tip for CodeWarrior TAP - not available for ordering anymore.

0 件の賞賛
返信
2,487件の閲覧回数
mbedardh
Contributor I

I need this probe tip also. Since it is not available anymore, please provide the pins numbers and signal names on CodeWarrier TAP so that I could make a custom compatible probe tip.

Thanks,

Michael

0 件の賞賛
返信
3,002件の閲覧回数
visakhanc
Contributor III

Thanks for your helpful reply.

Regards,

Visakhan

0 件の賞賛
返信