Compatible JTAG probe for MPC885

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compatible JTAG probe for MPC885

Jump to solution
3,269 Views
visakhanc
Contributor III

Hi all,

     I have a project based on MPC885c PowerQUICK processor. What is the supported Codewarrior TAP and Probe part number for this processor? I have the base unit CWH-CTP-BASE-HE and probe tip: CWH-CTP-COP-YE. Are these compatible with MPC885 ?

Regards

Visakhan

0 Kudos
Reply
1 Solution
3,076 Views
alexander_yakov
NXP Employee
NXP Employee

MPC8xx (PowerQuicc 1) devices have another type debug interface - BDM

For these device please order the following debug probe:

USB TAP for DPI Power Architecture|Freescale

CodeWarrior TAP with COP-type probe tip CWH-CTP-COP-YE - will not work. BDM-type probe tip for CodeWarrior TAP - not available for ordering anymore.

View solution in original post

0 Kudos
Reply
3 Replies
3,077 Views
alexander_yakov
NXP Employee
NXP Employee

MPC8xx (PowerQuicc 1) devices have another type debug interface - BDM

For these device please order the following debug probe:

USB TAP for DPI Power Architecture|Freescale

CodeWarrior TAP with COP-type probe tip CWH-CTP-COP-YE - will not work. BDM-type probe tip for CodeWarrior TAP - not available for ordering anymore.

0 Kudos
Reply
2,561 Views
mbedardh
Contributor I

I need this probe tip also. Since it is not available anymore, please provide the pins numbers and signal names on CodeWarrier TAP so that I could make a custom compatible probe tip.

Thanks,

Michael

0 Kudos
Reply
3,076 Views
visakhanc
Contributor III

Thanks for your helpful reply.

Regards,

Visakhan

0 Kudos
Reply