Compatibility between different MPC8309 core frequency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compatibility between different MPC8309 core frequency

1,438件の閲覧回数
brunoschmitt
Contributor I

I would like to know if part MPC8309CVMAGDCA (which runs at 400MHz) is 100% compatible with the MPC8309VMADDCA (which runs at 266MHz)? By compatible I mean if I just replace the 266MHz one by the 400MHz all functionalities will be the same, or it is needed to change any component around it (crystal and so on).

Thanks in advance!

ラベル(3)
0 件の賞賛
返信
1 返信

1,295件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Yes, they are 10% compatible. If you just replace 266 Mhz part by 400 Mhz part in 266 Mhz design, it will work at 266 Mhz without any changes required.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信