Can not find file "u-boot-2010.06-mpc8306som-support-v2.patch" when running "./ltib"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not find file "u-boot-2010.06-mpc8306som-support-v2.patch" when running "./ltib"

1,505 Views
maojiu
Contributor I

It can not find the files "u-boot-2010.06-mpc8306som-support-v2.patch.md5" and "u-boot-2010.06-mpc8306som-support-v2.patch" when running "./ltib". They are not in "www.bitshrine.org/gpp", though they are supposed to be there according to the output messages after running the command "./ltib". Where can I find the two files?

Tags (3)
0 Kudos
Reply
2 Replies

1,333 Views
yipingwang
NXP TechSupport
NXP TechSupport

Which Linux BSP ISO did you install?

Actually in the u-boot spec u-boot-2010.06-mpc8306som.spec.in, there is no this patch u-boot-2010.06-mpc8306som-support-v2.patch listed.

Thanks,

Yiping

1,333 Views
maojiu
Contributor I

Thank you for your reply. Finally I find the patch.

0 Kudos
Reply