CWH-CTP-BASE-HE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CWH-CTP-BASE-HE

2,707 Views
chuwenli
Contributor I

The download speed of CWH-CTP-BASE-HE G version is very fast. Now it's changed to the H version, which is very slow Do you need to upgrade the firmware? If you need to upgrade the firmware, where can I get the firmware upgrade?

Labels (2)
Tags (1)
0 Kudos
Reply
2 Replies

2,693 Views
yipingwang
NXP TechSupport
NXP TechSupport

No need to change the firmware of CodeWarrior TAP.

If you use Layerscape processor, please install the latest CodeWarrior for ARMv8 11.5.12.

925 Views
Guystg
Contributor I

Thank you,
A lot faster (15min to 10sec download at full clock speed) 

0 Kudos
Reply