phase error for gd3000

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

phase error for gd3000

4,247 次查看
steven_zhang
Contributor V

 I got "phase error" while i tred to run  a bldc witch runs at above 35000 N,i measure the PWM IN wave for gd3000 and PWM out from GD3000 ,i fount the out put from GD3000 for upper  mosfet is wrong which combines the PWM for  lower  MOSFET,it is real strange. for detail ,please see the atatchment.

标记 (1)
0 项奖励
回复
4 回复数

3,547 次查看
Jack_cheng
Contributor II
hi zhang,what type of BLDC do you used in your project sensorless or sensor?
For the world u are someone,but for someone u are the world
0 项奖励
回复

4,112 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Please also post your schematic here.

0 项奖励
回复

4,112 次查看
steven_zhang
Contributor V

my customer used the MOTORGD FRDM board ,he connect his STM32F429 evk  board and the MOTORGD with some Dupont Lines.the attachment is the  MOTORGD  sch. he cut the PCB trace between the two pins of J15 ,so he can drive his 24V BLDC motor , the 5V power supplier is power by the STM32F429 board .

0 项奖励
回复

4,112 次查看
guoweisun
NXP TechSupport
NXP TechSupport

如果是速度慢下来以后还会有这种错误发生吗?

0 项奖励
回复