Wireless Charging Coil Array Solution?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wireless Charging Coil Array Solution?

Jump to solution
7,203 Views
corynrobinson
Contributor I

Does NXP offer a solution for large area wireless charging? More specifically, I’d like to implement something similar to WPC’s B1 coil array. The part I’m having trouble with is coil selection.

Tags (2)
0 Kudos
Reply
1 Solution
6,933 Views
reyes
NXP TechSupport
NXP TechSupport

Unfortunately there is no solution in the current NXP portfolio to support 12 coils.

View solution in original post

0 Kudos
Reply
4 Replies
3,089 Views
Rixcyshah
Contributor I

If you’re trying to implement something similar to a WPC B1-style coil array for a large charging surface, coil selection can definitely be tricky. From what I’ve seen in Qi designs, parameters like coil diameter, inductance (typically around a few µH), Q-factor, and coupling efficiency with the receiver are critical for stable power transfer. Many multi-coil pads use overlapping PCB coils or pre-wound litz wire coils combined with a controller that can dynamically select the active coil depending on the receiver position. In practice, designers often prototype with a few coil geometries first and then optimize spacing and shielding to reduce cross-coupling between adjacent coils. Another approach I’ve noticed is using ready made wireless charging coils that are designed for Qi transmitters, since they already have tuned inductance and consistent manufacturing tolerances. That can simplify early prototyping before committing to a custom PCB coil array.

0 Kudos
Reply
6,933 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

I suggest you to use the WCT1111 in B type (Multi-coil) solution, this way you will use only one chip to control multiple coils.

Please refert to the detali in below link:/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fproducts%2Fpower-management%2Fwireless-power%2F1...https://www.nxp.com/products/power-management/wireless-power/15-watt-wireless-charging-transmitter-i...

I also recommend you to review the application note “Migration from A13 to B5 Wireless Charging Transmitter” in the link below, this App Note describes how to design a multiple coil wireless charger with the topology B5, which design has four PCB coils. This transmitter topology allows to connect two coils simultaneously to achieve better charging performance and active area efficiency for the case when the receiver is placed between two coils.

AN5059: https://www.nxp.com/docs/en/application-note/AN5059.pdf

Have a great day,

Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
6,933 Views
corynrobinson
Contributor I

Thank you for those resources, however, I’m looking for a solution that provides a much wider charging area. B5 only supports 4 coils, but I’d like to implement something like 12 coils.

0 Kudos
Reply
6,933 Views
reyes
NXP TechSupport
NXP TechSupport

Unfortunately there is no solution in the current NXP portfolio to support 12 coils.

0 Kudos
Reply