Voltage Stability Issue between FS6523 SBC and MC33665A TPL Transceiver VDDIO Connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Voltage Stability Issue between FS6523 SBC and MC33665A TPL Transceiver VDDIO Connection

1,116件の閲覧回数
Jamie-Chen
Contributor I

I am working on a circuit board design that includes an FS6523 SBC and an MC33665A TPL Transceiver. Currently, the SBC's VCCA output is set to 3.3V and is directly connected to the TPL Transceiver's VDDIO.

However, I am observing an issue where the VCCA output voltage increases to around 3.38V - 3.46V when the TPL Transceiver is connected. When the TPL is removed from the circuit, the voltage stabilizes back at 3.3V.

I would like to ask if it is acceptable for the SBC’s LDO to be directly connected to the VDDIO of the MC33665A TPL Transceiver, or if this could be causing the observed voltage increase.

Additionally, I noticed in the HVBMS RD-K358BMU reference design that two 22-ohm resistors are placed in series with the 3.3V LDO output from the SBC. Could these resistors be included to prevent voltage rise?

JamieChen_0-1731493959566.png

 

 

Thank you for your assistance.

ラベル(2)
0 件の賞賛
返信
1 返信

1,109件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Ivan (@ivanlovas), Amélie (@AmMeyer), 

Could one of you please help with request from XING Mobility Taiwan?

Thanks & BRs, Tomas

0 件の賞賛
返信