Verifying the SBCFS26 OTP Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Verifying the SBCFS26 OTP Configuration

Jump to solution
2,157 Views
Sivahari
Contributor I

Hi Nxp,

I am using SBC MFS2613AMDA6. 

I am aware that OTP Configuration can be done using a separate tool by changing voltage in debug pin. Is it possible to read OTP Configuration as like reading the Failsafe registers?

If I could be able to read the OTP configuration then where i can refer the address of those registers?

 

Thanks for your support.

0 Kudos
Reply
1 Solution
2,106 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

The FS26 provides an OTP readback mechanism only in Test/OTP mode, using mirror registers. This mechanism is intended for manufacturing, ATE and OTP programming verification and is not available during normal operation.

As I mentioned earlier, for the MFS2613AMDA6 the OTP configuration is fixed and the authoritative reference is the provided Configuration Report.

BRs, Tomas

View solution in original post

0 Kudos
Reply
4 Replies
2,139 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

For the MFS2613AMDA6, which is our standard pre‑programmed FS26 device, the OTP configuration is fixed at production.

The complete OTP configuration for this device is documented in the attached Configuration Report, which summarizes all OTP‑defined parameters.

BRs, Tomas

0 Kudos
Reply
2,134 Views
Sivahari
Contributor I

Hi Tomas,

It is really good to read OTP Configurations manually and understand the threshold value for each fault like (OV, UV etc).

But Is it possible to read those configurations through SPI as like fail safe/main register?

 

Thanks for clarifications.

0 Kudos
Reply
2,107 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

The FS26 provides an OTP readback mechanism only in Test/OTP mode, using mirror registers. This mechanism is intended for manufacturing, ATE and OTP programming verification and is not available during normal operation.

As I mentioned earlier, for the MFS2613AMDA6 the OTP configuration is fixed and the authoritative reference is the provided Configuration Report.

BRs, Tomas

0 Kudos
Reply
2,098 Views
Sivahari
Contributor I
Thank you for clarification.
0 Kudos
Reply