TEA2017 PFC Startup Limitation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TEA2017 PFC Startup Limitation

4,389 Views
cduignanvox
Contributor II

Hello,

I have an issue in a prototype using the TEA2017AAT/2 where the PFC stage seems to limit the current during startup for approximately 900ms after the input is applied:

CH1: PFC Vout
CH2: LLC Vout
CH3: Vin
CH4: Iin

120Vin, 100% power:

cduignanvox_0-1697553008006.png

Startup is interrupted as the PFC output voltage does not regulate properly until around 1s.

 

220Vin, 100% power:

cduignanvox_1-1697553085748.png

The PFC stage is able to regulate here because the current draw is lower. However, the change in behaviour can still be seen after 900ms.

 

The peak of the input current increases after approximately 900ms from when the input is applied, and then the converter behaves as normal.

cduignanvox_2-1697553254576.png

Left of the cursor is the current is flattened, right is normal.

The controller has been programmed to operate in DCM/QR mode.

 

Is there anything inside the TEA2017 which would match this timing? Why is the PFC stage limiting the current?

Thanks,

Connor

 

 

 

 

Tags (2)
0 Kudos
Reply
3 Replies

4,366 Views
guoweisun
NXP TechSupport
NXP TechSupport

If you disable LLC part only debug PFC part, does this still happen?

 

0 Kudos
Reply

4,356 Views
cduignanvox
Contributor II

Hi guoweisun,

I disabled the LLC stage and supplied the TEA2017 SUPIC pin through a diode with 20V due to the absence of switching on the auxiliary winding.

I tried to match the same output power as when the LLC stage was running.

220Vin, 100% power:

cduignanvox_0-1697629031467.pngcduignanvox_1-1697629083810.png

The flattening of the input current is still happening, and the timing is the same.

One thing to note is that the consistent timing of ~900ms is from when the input voltage is applied, not when the PFC stage starts. Due to the 20V on SUPIC the PFC stage starts as soon as input is applied, but in the test with the LLC stage running the SUPIC pin needs to charge before the PFC stage starts, yet the timing of this anomaly is the same.

Thanks,

Connor

0 Kudos
Reply

4,340 Views
guoweisun
NXP TechSupport
NXP TechSupport

I give your TEA2017 calculation sheet here, please double check your schematic  about PFC design part especially -4 Sense resistor selection.

Hope this could help you!

0 Kudos
Reply