Replacement part for PCA9460

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Replacement part for PCA9460

1,449 Views
Cécile__
Contributor II

Hello,

I'm designing a board based on the IM8ULP. In the hardware recommandations, the vias size used is standard (~0.4mm diam / 0.2mm hole, tht). However, for the PMIC part (PCA9460), some microvias/blinvias are used...

Therefore, I'm searching a PMIC with a larger package, to use the same vias size.

Which one could I use for this application ?

Thank you for your help,

CJ

0 Kudos
Reply
2 Replies

1,421 Views
Cécile__
Contributor II

Hello,

Thank your for your help, I will search another reference !

Regards,

Cécile J

0 Kudos
Reply

1,433 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Cécile__,

I hope all is great with you. Thank you for using the NXP communities.

I am afraid that within the PCA9460 series, the only available package is WLCSP42. Please accept my apologies.

diazmarin09_0-1717107244579.png

 

The only solution that comes to my mind, is to select a non-programmed PMIC from another series, to program it and try to emulate the behavior of the PCA9460 series.

I hope this information helps.

Regards,

David

0 Kudos
Reply