Replacement part for PCA9460

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Replacement part for PCA9460

1,520 次查看
Cécile__
Contributor II

Hello,

I'm designing a board based on the IM8ULP. In the hardware recommandations, the vias size used is standard (~0.4mm diam / 0.2mm hole, tht). However, for the PMIC part (PCA9460), some microvias/blinvias are used...

Therefore, I'm searching a PMIC with a larger package, to use the same vias size.

Which one could I use for this application ?

Thank you for your help,

CJ

0 项奖励
回复
2 回复数

1,492 次查看
Cécile__
Contributor II

Hello,

Thank your for your help, I will search another reference !

Regards,

Cécile J

0 项奖励
回复

1,504 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Cécile__,

I hope all is great with you. Thank you for using the NXP communities.

I am afraid that within the PCA9460 series, the only available package is WLCSP42. Please accept my apologies.

diazmarin09_0-1717107244579.png

 

The only solution that comes to my mind, is to select a non-programmed PMIC from another series, to program it and try to emulate the behavior of the PCA9460 series.

I hope this information helps.

Regards,

David

0 项奖励
回复