RD33771CDSTEVB - using with 8 cells

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RD33771CDSTEVB - using with 8 cells

1,315件の閲覧回数
Gad_usr1
Contributor II

Hi, I am using RD33771CDSTEVB. To use this board for 8 cells instead of 14 cells, we followed the table below and shorted the unused pins to cell 4. But we are getting wrong values. It is working when we are reading 14 cells. Kindly suggest if any further modification needs to be done in software or hardware

Gad_usr1_0-1721909251504.pngGad_usr1_0-1721909251504.png

Gad_usr1_1-1721909381585.pngGad_usr1_1-1721909381585.png

 

 

0 件の賞賛
返信
2 返答(返信)

1,312件の閲覧回数
Gad_usr1
Contributor II

we used filter type c 

Gad_usr1_0-1721909645021.pngGad_usr1_0-1721909645021.png

 

0 件の賞賛
返信

1,284件の閲覧回数
Gad_usr1
Contributor II

Below shows the cell voltage readings. Total stack voltage is correct. Also voltages of cell 3,4,11 and 12 are correct. But cell 1, 2, 13, 14 are wrong. These cells are also around 3.2V when checked with multimeter.

Gad_usr1_0-1721984147321.pngGad_usr1_0-1721984147321.png

 

0 件の賞賛
返信