Programming ROM writer equipment of MMPF0100NP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming ROM writer equipment of MMPF0100NP

2,242件の閲覧回数
thc_syn
Contributor I
I will use the programming ROM writer equipment of ELNEC to write the configuration data in MMPF0100NPAEP.
I heard that using the ELNEC programmer there are cases where verify can not be used.
Could you please tell me this results and problems of this cases used with these combinations.
<Our case>

-ELNEC Programmer : BeeHive204

https://www.elnec.com/en/products/production-programmers/beehive204/

 

-Programming adapter : DIL48/QFN56-2.02 ZIF PMIC-1

  (specialized adapter for Freescale PF series of PMICs devices (PF0100,PF0200) in QFN56 package)

https://www.elnec.com/en/products/programming-adapters/DIL48_QFN56-2.02_ZIF_PMIC-1/

 

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,101件の閲覧回数
thc_syn
Contributor I

Hi Jose,

Thank you for your answer.
I have a PF series programmer but I am considering a mass production ROM writer.
I will check ELNEC for more details on MMPF 0100 writer.

Best regards,

0 件の賞賛
返信

2,101件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

I checked our support database and we have not received any case with an issue programming or verifying the programming of the PF0100 using the ELNEC programmer. And even if you have a problem with it, we cannot provide support since the ELNEC Programmer: BeeHive204 and the Programming adapter: DIL48/QFN56-2.02 ZIF PMIC-1 were not designed by NXP, you would need to contact ELNEC directly.

 

My responsibility as NXP is to recommend you to use the PF programmer from NXP instead to program your PMIC, you can find it in the following links:

PF Series Programmer: https://www.nxp.com/support/developer-resources/evaluation-and-development-boards/analog-toolbox/pf-...

 

 OTP Programming Socket: https://www.nxp.com/support/developer-resources/evaluation-and-development-boards/analog-toolbox/eva...


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信