Programming ROM writer equipment of MMPF0100NP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming ROM writer equipment of MMPF0100NP

2,825 Views
thc_syn
Contributor I
I will use the programming ROM writer equipment of ELNEC to write the configuration data in MMPF0100NPAEP.
I heard that using the ELNEC programmer there are cases where verify can not be used.
Could you please tell me this results and problems of this cases used with these combinations.
<Our case>

-ELNEC Programmer : BeeHive204

https://www.elnec.com/en/products/production-programmers/beehive204/

 

-Programming adapter : DIL48/QFN56-2.02 ZIF PMIC-1

  (specialized adapter for Freescale PF series of PMICs devices (PF0100,PF0200) in QFN56 package)

https://www.elnec.com/en/products/programming-adapters/DIL48_QFN56-2.02_ZIF_PMIC-1/

 

Labels (1)
0 Kudos
Reply
2 Replies

2,684 Views
thc_syn
Contributor I

Hi Jose,

Thank you for your answer.
I have a PF series programmer but I am considering a mass production ROM writer.
I will check ELNEC for more details on MMPF 0100 writer.

Best regards,

0 Kudos
Reply

2,684 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

I checked our support database and we have not received any case with an issue programming or verifying the programming of the PF0100 using the ELNEC programmer. And even if you have a problem with it, we cannot provide support since the ELNEC Programmer: BeeHive204 and the Programming adapter: DIL48/QFN56-2.02 ZIF PMIC-1 were not designed by NXP, you would need to contact ELNEC directly.

 

My responsibility as NXP is to recommend you to use the PF programmer from NXP instead to program your PMIC, you can find it in the following links:

PF Series Programmer: https://www.nxp.com/support/developer-resources/evaluation-and-development-boards/analog-toolbox/pf-...

 

 OTP Programming Socket: https://www.nxp.com/support/developer-resources/evaluation-and-development-boards/analog-toolbox/eva...


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply