Powering RFEM24-250

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Powering RFEM24-250

2,473 Views
bell-r21
Contributor I

I am looking to power a RFEM24-250 using a battery, can you advise which voltage of battery would be required?

Thanks

Tags (1)
0 Kudos
Reply
1 Reply

2,398 Views
LPP
NXP Employee
NXP Employee

The RFEM24-250 requires +30V (500W) and +5V power supply.

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply