PMIC for fpga

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PMIC for fpga

2,549件の閲覧回数
Michaelscott237
Contributor I

Hey, i have board which integrates two  fpga's which needs several different voltages.

My main power is 12v

The first is fpga requires  1.2v for core and 3.3v for vccio and the second is  requires 1.0 for core, 3.3 for some vccio, 1.0v for serdes core, 1.8 for aux and 1.1v for some vccio (for lpddr) 

So i will need buck converters and ldo's for the serdes and aux power. I also need to power lpddr4 which for that i use a ti pmic which requires 5v and input that can be received from my main power. 

For now i used lt8653 converters and tps74901 ldo's to power everything but i wanted to know if you have a PMIC to replace all this power system that can fit for my requirements.

Thanks in advance

0 件の賞賛
返信
4 返答(返信)

2,530件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi Michael

What are the loading capability for each regulators your required?

0 件の賞賛
返信

2,514件の閲覧回数
Michaelscott237
Contributor I
Hey,
First fpga required 1.2v and 3.3v and has about 40mW power consumption.
Second fpga requires 1.0v core, 1.8v aux, 1.0v and 1.8v for serdes core and aux and 3.3/1.1 for io.
Power consumption around 500mW.
Enet phy requires 400mW.
Lpddr pmic requires 5v and 4-18v input.
Consumption around 200mW.

Regulators will power only serdes block and core voltages
0 件の賞賛
返信

2,495件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

1:For the 5V input I recommend MC34PF8100.

 

0 件の賞賛
返信

2,462件の閲覧回数
Michaelscott237
Contributor I
Thanks, but its overkill for my design.
Thanks anyway
0 件の賞賛
返信