Hello,
PMIC PF3000 Datasheet contains the following comments regarding voltage drop
for the SW2:
The higher output voltages available depend on the voltage drop in the conduction path as given
by the following equation: (VSW2IN - VSW2) = ISW2* (DCR of Inductor +RONSW2P + PCB trace
resistance).
The similar statement, which allows to estimate minimal input voltage, is also for the SW3;
but there is no such equation for the SW1. What are considerations for the SW1?
https://www.nxp.com/docs/en/data-sheet/PF3000.pdf
Regards,
Yuri.
解決済! 解決策の投稿を見る。
Hi
In set down regulator equation: (VSW2IN - VSW2) = ISW2* (DCR of Inductor +RONSW2P + PCB trace
resistance).
The conditions of entry into force that equation is in the bypass mode the 100% duty cycle under VIN very near with VOUT.
This equation can be used in each set down regulator same with SW1/2/3 if Vout is very near with VIN.
Hello, guoweisun
The equation
(VSW2IN - VSW2) = ISW2* (DCR of Inductor +RONSW2P + PCB trace resistance)
relates to SW2.
Is the same correct for the SW1 ?
Regards,
Yuri.
Sure,same with SW1.