PMIC PF3001: value of Vin (min), when Vout is 3.3V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PMIC PF3001: value of Vin (min), when Vout is 3.3V

Jump to solution
2,608 Views
Yuri
NXP Employee
NXP Employee

Hello,

   PMIC PF3000 Datasheet contains the following comments regarding voltage drop

for the SW2:

  The higher output voltages available depend on the voltage drop in the conduction path as given

by the following equation: (VSW2IN - VSW2) = ISW2* (DCR of Inductor +RONSW2P + PCB trace

resistance).

 The similar statement, which allows to estimate minimal input voltage, is also for the SW3;

but there is no such equation for the SW1. What are considerations for the SW1?    

https://www.nxp.com/docs/en/data-sheet/PF3000.pdf 

Regards,

Yuri.

Labels (1)
0 Kudos
Reply
1 Solution
2,434 Views
guoweisun
NXP TechSupport
NXP TechSupport

Sure,same with SW1.

View solution in original post

0 Kudos
Reply
3 Replies
2,434 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

In set down regulator equation: (VSW2IN - VSW2) = ISW2* (DCR of Inductor +RONSW2P + PCB trace

resistance).

The conditions of entry into force that equation is in the bypass mode the 100% duty cycle under VIN very near with VOUT.

This equation can be used in each set down regulator same with SW1/2/3 if Vout is very near with VIN.

0 Kudos
Reply
2,434 Views
Yuri
NXP Employee
NXP Employee

Hello,  

 The equation 

(VSW2IN - VSW2) = ISW2* (DCR of Inductor +RONSW2P + PCB trace resistance)

relates to SW2.

  Is the same correct for the SW1 ?

  

Regards,

Yuri.

0 Kudos
Reply
2,435 Views
guoweisun
NXP TechSupport
NXP TechSupport

Sure,same with SW1.

0 Kudos
Reply