PF8100 VDDIO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF8100 VDDIO

2,318件の閲覧回数
ceng_guanghui
Contributor II

I want to confirm that the PF8100_VDDIO powered by Its own buck,What's the difference ,compared with use external power.

Thanks.

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

2,239件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Please read datasheet page16--

13.1.4 QPU_Off state
The QPU_Off state is a higher power consumption off mode, in which all internal circuitry
required for a power on is biased and ready to start a power up sequence.
If LPM_OFF = 1 and no turn on event is present, the device stops at the QPU_Off state,
and waits until a valid turn on event is present.
In this state, if VDDIO supply is provided externally, the device is able to communicate
through I2C to access and modify the mirror registers in order to operate the device in
TBB mode or to program the OTP registers as described in Section 17 "OTP/TBB and
default configurations".

0 件の賞賛
返信