PF3000 front-end input LDO regulator issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PF3000 front-end input LDO regulator issue

10,638 次查看
prezek
Contributor II

 

We have some issue with PMIC PF3000. It appears only occasionally, but it is a big issue for us. If it happens, we are not able to get out of the error state.

The issue:

5V is provided to pin VPWR, but VIN genertes only 1.5V - 1.8V

I think the problem is caused by not activating external PMOS pass FET MP1. (see attached Figure 3)

 

Additional info:

Figures form startup sequence:

Yellow - VPWR

Light blue - VIN

Purple - LDOG

Figure 1: Correct startup waveforms (the purple signal is partly hidden by the yellow one)Figure 1: Correct startup waveforms (the purple signal is partly hidden by the yellow one)

Figure 2: Failure startup waveforms (the purple signal is hidden by the yellow one)Figure 2: Failure startup waveforms (the purple signal is hidden by the yellow one)

Figure 3: Detail on failure startup waveformsFigure 3: Detail on failure startup waveforms

Voltage measured on PMIC pins:

1INTB0.3V
2SD_VSEL0V
3RESETBMCU0V
4STANDBY0V
5ICTEST0V
6SW1AFB0.3V
7SW1AIN1.5V
8SW1ALX0.3V
9SW1BLX0.011V
10SW1BIN

1.5V

11SW1BFB

0.011V

12GNDREF1

0V

13VLDO1IN

1.5V

14VLDO1

0.54V

15VLDO2

0.11V - 0.44V

16VLDO2IN

0V

17SW2LX

0V

18SW2IN

1.5V

19SW2FB

0V

20VLDO3

0.024V

21VLDO34IN

1.5V

22VLDO4

0.02V

23VHALF

0V

24VINREFDDR

0V

25VREFDDR

0V

26GNDREF2

0V

27SW3FB

0V

28SW3IN

1.5V

29SW3LX

0V

30LDOG

4.97V

31VPWR

4.98V

32V33

0V

33VCC_SD

0V

34VSNVS

0.68V

35SWBSTLX

1.5V

36LICELL

1.17V

37SWBSTFB

1.2V

38VIN2

1.5V

39VDDOTP

0V

40GNDREF

0V

41VCORE

0V

42VIN

1.5V

43VCOREDIG

0.94V

44VCOREREF

1.08V

45SDA

0.3V

46SCL

0.3V

47VDDIO

0.3V

48PWRON

2.75V

 

标签 (1)
0 项奖励
回复
14 回复数

10,551 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Petr,

what PFET have you used? Please refer to section 4 in the AN5161. FDMA908PZ is recommended to be used. I would also like to point you to AN5094 Layout guidelines. Both application notes can be downloaded from this link. 

JozefKozon_0-1645711847518.png

With Best Regards,
Jozef

 

0 项奖励
回复

10,538 次查看
prezek
Contributor II

Hello Jozef,

thank you for your reply.

We are using PFET PMPB15XP (it's recommended by the datasheet).

I don't think that the transistor could cause the issue. If you look on the waveforms, you can see, that PMIC doesn't try to open the gate of the transistor.

 

Figure 4: schematics of our circuitFigure 4: schematics of our circuit

 

0 项奖励
回复

10,496 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Petr,

thank you for the PFET confirmation and for the schematic. I have found a thread where a customer had a similar issue. The reason was another load connected to the VIN pin. But I see from the schematic, that you haven't anything other connected to the VIN pin. I have posted the description of your issue to our application team. As soon as I will receive an answer, I will definitely reply to you. 

With Best Regards,

Jozef

0 项奖励
回复

10,459 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Petr,

there is still no answer from the application team. As soon as I will receive one I will definitely reply to you.

Thank you for your patience. 

With Best Regards,

Jozef

0 项奖励
回复

10,428 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Petr,

I have just received an answer from the application engineer. He asks me to confirm with you, that there is no other load connected to the VIN pin. Although from your schematic I see, that there is no other load connected, could you please confirm it?

With Best Regards,

Jozef

0 项奖励
回复

10,425 次查看
prezek
Contributor II

Hi Jozef,

I confirm that we are not using the VIN net for anything else then suppling the PF3000. Everything connected to the signal is showed on the schematic above.

 

I have tried 2 things if the error state could be forced by increasing load on VIN:

  • I have tried adding additional capacitor between VIN and GND – I didn’t see any difference

 

  • I have tried adding resistor load between VIN and GND:

       - with 1 k there was no difference

       - with 100 ohm additional load there VIN signal was not stable until the external FET was activated

I was not able to increase occurrence of the error state by additional load          

 

I would like to ask you how the start of using the external FET is timed. It looks like it takes approx. 400ms. Is the timing block supplied from VIN or VPWR?

Could you share any details about generating VIN before external FET is activated? (current limitation, timing, reference sources etc.)

 

Thank you, Petr

10,367 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Petr,

I have posted your confirmation to the application engineer, but I haven't received an answer from him yet. I have added another application engineer in the communication loop. As soon as I will receive an answer from either of them, I will definitely reply to you.

Thank you for your patience.

With Best Regards,

Jozef

0 项奖励
回复

10,357 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Petr,

the added application engineer has just answered me. He requests to measure the VPWR current when the fault happens.

DESCRIPTION

Its hard to say what’s going on. Could there be a current limit at the VIN node?

When in this problem state, what is the current drawn from VPWR?

With Best Regards,

Jozef

0 项奖励
回复

10,350 次查看
prezek
Contributor II

Hi Jozef,

we have installed a current probe to the device. 

It measures current drawn from VPWR and charging current of filtering capacitors. We are not able to separate the capacitors from VPWR.

Yellow - current

Green - VPWR (partially hidden by LDOG)

Blue - VIN

Ping -LDOG

Figure 5: Correct startup waveformFigure 5: Correct startup waveform

Figure 6: Faulty state startup waveformFigure 6: Faulty state startup waveform

Figure 7: Detail on faulty startup waveformFigure 7: Detail on faulty startup waveform

 

I have one potentially useful information:

When we disconnect power supply, the voltage on VIN falls very slowly (because of the capacitors) and if we reconnect power supply, the PMIC stays in the error state. The voltage can fall bellow 0.4 V and it stays in error state (tens of seconds without power supply).

Figure 8: Power supply disabled for 22s, VIN drops to 0.23 V, PMIC stays in error stateFigure 8: Power supply disabled for 22s, VIN drops to 0.23 V, PMIC stays in error state

When we disconnect power supply for longer time, PMIC usually starts correctly.

 

Is the PMIC internally powered from VIN or some other pin? I could measure voltage on any pin...

 

10,303 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Petr,

please see below an answer from the application engineer with a suggestion.

DESCRIPTION

I am not sure if the PMIC is getting stuck in some weird state due to startup from a non-discharged VPWR. Is it possible to add a small bleeder resistor from VPWR to ground to allow it to discharge faster, and see if the problem resolves?

With Best Regards,

Jozef

0 项奖励
回复

10,294 次查看
prezek
Contributor II

Hi Jozef,

I have induced the issue and then I have tried 2 experiments and added 100 ohm resistor in 2 places:

1. Between VPWR and GND

2. Between VIN and GND

Then I disconnected power supply. In both cases the corresponding voltage dropped very quickly below 1mV. After reconnecting power supply the error state continued in both cases.

Discharging resistor on VPWR or VIN dos not help.

 

Could you please tell me which pin is supplying the logic, timing, etc. of driving LDOG and internal states?

0 项奖励
回复

10,279 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Petr,

please send the board for debugging to the application engineer. I will pass the application engineer's details to in the ticket. Please see the application engineer's reply below.

DESCRIPTION

I believe there is a path from VPWR that powers logic, bandgap etc.

I think best may be to send a board to Bruce in TJN for debug.

 

With Best Regards,

Jozef

0 项奖励
回复

10,038 次查看
prezek
Contributor II

Hi Jozef,

I tried to create a tool for simple enforcing the issue for you. I noticed that the issue occurs when I power up the PMIC, then unplug the power for approx. 10 minutes and then re-enable power.

I measured which voltage is discharged so slowly and found out that SWBSTFB has 0.2 V 10 minutes after disconnecting the power.

Then I found out that I can force the error state by charging capacitors connected to SWBSTFB to 0.25 V before connecting the PMIC to the power supply.

 

After we added 1 k resistor parallel to the capacitors on SWBSTFB signal, the issue never occurred.

 

I don`t see any reason for this behaviour in the datasheet of PF3000.

Can you please confirm that 0.2 V on SWBSTFB can be the cause of the error and explain it? 

Will there be any revision with correction of this issue?

 

Thank you, Petr

0 项奖励
回复

9,998 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Petr,

I have received an answer from the application engineer. He tried to reproduce the issue on our PF3000EVB, but there wasn't voltage on the SWBSTFB as in your case. It looks like in the case of our PF3000EVB, the energy is dissipated, but in case of your board, the energy stays accumulated in the capacitor. I have checked your schematic and its correct. Please check an AN5094 attached and please follow the layout recommendations. You can also refer to the Gerber files of the KITPF3000FRDMEVM.zip attached. Please consider purchase the KITPF3000FRDMEVM and FRDM-KL25Z for evaluation.

With Best Regards,

Jozef

0 项奖励
回复