PF1550 OTP Programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF1550 OTP Programming

1,044件の閲覧回数
trung1
Contributor I

Hi,

I am working with non-programmed part PF1550. I have read its datasheet and the OTP programming Instructions AN12408. But when trying to follow the programming example, I encounter some weird register addresses like 0xC0, 0xC1, 0xC2,..., for which I cannot find descriptions. Which documents should I read to find these registers?

Example instructions from AN12408:

...
//===========================================================================
// Commands are for OTP programming setting
//===========================================================================
WRITE_OTP_CONTROLLER:PMIC:0xC0:0xA5
WRITE_OTP_CONTROLLER:PMIC:0xC1:0x1C
WRITE_OTP_CONTROLLER:PMIC:0xC2:0x38
WRITE_OTP_CONTROLLER:PMIC:0xC8:0x0F
WRITE_OTP_CONTROLLER:PMIC:0xC9:0x02
WRITE_OTP_CONTROLLER:PMIC:0xCA:0x07
WRITE_OTP_CONTROLLER:PMIC:0xCD:0x35
EXEC_DELAY:1000
WRITE_OTP_CONTROLLER:PMIC:0xC0:0x96
EXEC_DELAY:200
READ_OTP_CONTROLLER:PMIC:0xC6
EXEC_DELAY:1000
WRITE_OTP_CONTROLLER:PMIC:0xC0:0x00
...

 

ラベル(1)
0 件の賞賛
返信
1 返信

1,004件の閲覧回数
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Could you please open a support ticket and upload the Excel file that contains the script generation for your reference?

https://www.nxp.com/support/support:SUPPORTHOME

Unfortunately, I’m unable to share it directly here.

Thank you!

0 件の賞賛
返信