PF1550 Battery Powerd

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PF1550 Battery Powerd

1,328 次查看
EngineerPMIC
Contributor I

Hi,

I want to use the PF1550 in a wearable device. When I am looking into the typical application circuit I see that VBUSIN is the default power input of the PF1550. If a battery is connected to VBATT and VBUSIN is removed. Will VBATT automatically take over and source VSYS? 

Typically I want a design with a battery powering VSYS and once in a while charge the battery by connecting USB to VBUSIN. 

Kind Regards

标记 (1)
0 项奖励
回复
1 回复

1,317 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Daan,

Yes, if the charger is removed from VBUSIN, then VBATT will automatically power VSYS without any interrupt. 

Best regards,

Tomas

0 项奖励
回复